What are Passive Components in Electronics?

Passive electronic components are devices that operate without requiring their own independent power source. They do not actively control or amplify an electrical signal, but instead respond to and influence the electricity already present in a circuit.

 

So, basically, passive electronic components operate from the electricity or energy already in the circuit it is on, as they cannot generate energy, and they are not sources of energy. A passive electronic component does not generate power, but instead dissipates, stores, and/or releases it.  Every electronic circuit is an arrangement of electrical components designed to perform specific functions - passive components can become an active part of a circuit in unexpected ways. Transformers, categorized as passive, can raise voltage, but since they do not raise or lower power or energy they are classified as a passive element. Similarly, capacitors limit the interaction of electricity as just storing it, not supplying it.


 

There are two basic types of passive electronic components:

  1. Dissipative or Lossy - these are predominantly resistors - components that does not have the ability to absorb any power from an external source.

  2. Lossless - these components have no output or input of power flow and include capacitors, transformers and inductors. But all passive components dissipate some power due to minor internal resistances - so are not 100% lossless.

 

The table below shows the main differences between passive and active electronic components.


 

 

Passive Components

Active Components

Power usage

Uses power in circuit

Delivers power to circuit

Nature of energy

Energy acceptor

Energy donor

Component function

Stores energy

Produces energy

Power gain

Cannot give power gain

Can provide power gain

Need external source

Does not need to operate

Needs to operate

Current flow

Cannot control flow of current

Can control flow of current

Examples

Resistor, Capacitor, Inductor, Transformers

Amplifiers, Transistors, Integrated circuits

 

To summarize, the major types of passive components each have their unique element that stamps them passive. Resistors, like the name states, resist current flow; capacitors store energy; inductors resist changes in energy flow; while transformers can influence voltage by increasing or decreasing it to meet the needs of the electronic device. So while passive, they can have action without being classified active.

 
您是否认为这篇文章有用?请分享!

Join the circuit, Keeping You Connected to OnlineComponents.com & Beyond!