help desk software

Why is Gallium Nitride (GaN) so Popular with New Power Supplies?

If you’ve recently looked at the marketing for a modern USB-C charger, telecom rectifier, or server power supply unit, you have likely seen three letters driving the design - GaN.  At OnlineComponents.com, where we support both design engineers and component buyers across industries, we’re seeing gallium nitride devices move from “unheard of” to “everywhere” in AC/DC and DC/DC power supplies as well as motor drivers.  Here’s why GaN has captured so much attention, and what to look for when you’re qualifying parts or building a bill of materials.

 

What GaN Brings to the Table

GaN is a wide-bandgap semiconductor with a much higher critical electric field and electron mobility than silicon.  In practice, that means transistors with lower capacitances, faster switching, and dramatically reduced switching losses compared to silicon MOSFETs.  Unlike silicon MOSFET body diodes, GaN power transistors don’t rely on minority carriers, so reverse-recovery charge is basically zero.  The physics behind these devices are the foundation for today’s smaller, cooler, and more efficient power supplies.

Designers typically turn to GaN for roughly the 100-650 volt range, compact phone and laptop chargers and many industrial power supplies.  For even higher voltages and larger power, silicon carbide is often the better fit, such as electric-vehicle drive inverters and the charger built into the car.  Both are next-generation semiconductor materials, but they excel in different ranges, which is why distributors usually offer options in both.

 

Efficiency and Power Density: Why Buyers Care

Because gallium nitride can switch quickly with low loss, designers push higher switching frequencies (often two to five times higher than that of silicon-based supplies.  That lets you shrink magnetics and capacitors, reduce heat-sink mass, and increase overall power density.  It is this technology that is behind those small form factor, high-power USB-C Power Delivery chargers and Power Supply Units that are becoming so popular.  With these high-frequency, high-voltage systems, you find significantly higher slew rates, with tens of volts per nanosecond being common, requiring reference designs that emphasize layout discipline to keep electromagnetic interference (EMI) in check.

All of these features lead to practical benefits for end-users.  Using gallium nitride, it is possible to achieve a lower system cost at the same, or even better, performance.  While a GaN device may be more expensive than a comparable silicon MOSFET, system cost often drops because you can downsize the magnetics (transformers and the like), capacitors, thermal hardware, and enclosure volume.  That’s a bill-of-materials conversation that modern power designers should be having with their systems designers daily.

The higher efficiency of these power supplies is an obvious path to equally higher efficiency certifications.  Data-center and PC power supplies compete on energy-efficiency labels and using GaN-based front-ends makes those targets easier by cutting PFC and primary-stage losses at partial and full load.

Finally, a product that is smaller and lighter is beneficial for everyone.  For adapters and embedded supplies, shipping weight, port density, and thermal comfort matter.  The benefits of GaN’s density are apparent to many and this benefit is visible on retail shelves where multi-port, 65-100 watt wall chargers are half the size of their silicon predecessors.  Indeed, if an end product uses the words “ultra-compact” or “pocket-sized” in its marketing, there’s a good chance that there’s gallium nitride inside.

 

Topology Trends with Gallium Nitride

There are a few topologies that are becoming more prevalent due to the features unique to GaN-based MOSFETs.  A newer style of power-factor correction replaces the usual input diode bridge.  The fast, clean switching makes this practical, so you get higher efficiency and fewer parts.  Skipping this diode bridge does require a careful circuit layout, good input filtering, and attention to current sensing and switch timing to keep electrical noise in check.

Whether you use a resonant converter or a simple half-bridge, GaN lets you switch faster with lower loss, meaning that you can use a high-frequency isolated stage.  That yields a smaller transformer and capacitor without giving up efficiency.  Many designers pair a Gallium Nitride front end with a GaN half-bridge so the whole primary side runs cooler and lighter.

On the secondary side, low-voltage step-down and step-up stages - something along the lines of 48 volts to 12 volts or 12 volts to 5 volts - reduce the energy wasted each time the switches turn on and off.  The result is compact, multi-output supplies that stay efficient even as the transformers become smaller.

Integrated GaN power stages are devices where the transistors are integrated with the driver and protection.  Integration shortens the sensitive wiring loops, making high-speed switching easier to control, often simplifying the PCB.  For many teams, this is the fastest path to a reliable, high-density design.

 

Reliability of GaN Transistors

Early skeptics of the GaN technology worried about the dynamic RDS(on) shifts, qualification methods, and long-term gate reliability.  In response to these concerns, the industry has standardized test and reporting practices and publishes application-relevant lifetime data.  When you evaluate parts, ask for stress conditions that resemble your use case and look for qualifications aligned to GaN-specific guidance rather than only legacy silicon MOSFET tests.

From a designer’s viewpoint, there’s a practical checklist of items to check or address we recommend to engineering and sourcing teams.  

  • Voltage class and topology fit. As most GaN today is ideal in the 100-650 V range, it only makes sense in applications that fall into that range.  Even after that, though, you will need to ensure that all other parameters fit your needs.
  • Integrated versus discrete driver.  Integrated GaN solutions, with driver and protection included, reduce parasitics and design risk.  Discrete GaN solutions, on the other hand, give you flexibility and may offer more package options.
  • Thermal protection.  Efficiency is higher than many other technologies but packages are smaller.  This makes it just as important to validate thermal paths.  As with all electronics, a cooler junction extends lifetime and avoids derating surprises.
  • Electromagnetic interference (EMI) strategy - Fast edges save watts but can emit undesired electromagnetic waves.  Budget for snubbers, spread-spectrum if possible, and simulate common-mode currents early to make certain the design will both function properly and not exceed emission requirements.
  • Supply chain and second-source.  As a distributor, we’re all too aware of the challenges of sourcing electronics components.  Fortunately, as GaN has grown in demand, it has become a multi-vendor market with multiple suppliers producing similar components.  



Summary

Gallium nitride’s rise is not hype.  It is a materials advantage turned into everyday design wins.  For engineers, it unlocks higher efficiency, higher frequency, and higher power density with mainstream tools and reference designs.  For buyers, it can lower system cost, reduce size and weight, and support aggressive efficiency roadmaps.  As you qualify your components, look for GaN-specific reliability data and confirm multi-supplier coverage to reduce the risk of your plan.

この記事はお役に立ちましたか?それを共有してください!