Microchip's New 64 Mbit Parallel SuperFlash® Memory

Microchip Technology’s series of radiation-tolerant COTS-based devices for space systems announced the addition of a 64 megabit parallel superflash memory, the company reported.

 

The memory complements Microchip’s COTS-based processors and its communication interfaces can be used to streamline space-qualified system development.

 

“To reduce the time, cost and risk of developing spaceflight-qualified systems, designers may start with Commercial-Off-The-Shelf (COTS) devices that can later be replaced by their space-qualified, radiation-tolerant equivalent parts available in plastic or ceramic packages featuring the same pinout distribution.  Microchip Technology Inc.  today announced a radiation-tolerant, 64 Megabit (Mbit) parallel-interface SuperFlash memory device with unrivaled Total Ionizing Dose (TID) tolerance for maximum reliability and robustness in the harsh radiation environment of space missions. It is an ideal companion to Microchip’s space-ready microcontrollers (MCUs), microprocessors (MPUs) and Field Programmable Gate Arrays (FPGAs) that provide the building blocks for this scalable development model,” Globe Write noted..   

Bob Vampola, associate vice president of Microchip’s aerospace and defense business unit, noted that the SST38LF6401RT SuperFlash device will strengthen the company’s scalable approach to developing total space system solutions that employ radiation-tolerant or radiation-hardened microprocessors and FPGAs.  “It offers the vital protection these space systems need for the most reliable digital processing where companion Flash memory is required to store the critical software code or bitstream that drives the complete system,” he added.

By allowing up to 50 kilorad (krad) TID radiation-tolerance while the Flash is still biased and operating, the SST38LF6401RT device enables systems to operate in a broad range of  space applications where any loss of code execution that could lead to severe defects and system loss cannot be allowed.

This makes the superflash memory an ideal companion to Microchip’s SAMRH71 Arm® Cortex®-M7-based radiation-hardened SoC processor and can also be used with the company’s RT PolarFire® FPGAs to support in-flight system reconfiguration. The device has pinout distribution compatibility with its industrial version for easy transition to the space-qualified plastic or ceramic versions at the Printed Circuit Board (PCB) level. Voltage operation of the SST38LF6401RT ranges from 3.0 to 3.6 volts (V).

Development Tools and Availability

The SST38LF6401RT SuperFlash device is sampling now in a ceramic version and supported by an evaluation board and demonstration software, available upon request. Also available upon request is an FPGA flight programming reference case for combining the SuperFlash device with an FPGA and a SAMRH71 processor with supporting software.

Microchip’s COTS-to-Radiation-Tolerant Process

By selecting relevant devices from its proven automotive- or industrial-qualified product family and adding silicon process improvements, Microchip gives them enhanced protections that make them more immune to single-event latch-up in heavy ion environments. The radiation performance of the slightly modified devices is fully characterized and supported by a dedicated radiation report for each functional block. The devices are used in applications ranging from launch vehicles and satellite constellations to space stations. Designers can begin system implementation with easy-to-source COTS devices before swapping them out with pinout-compatible space-qualified equivalents in high-reliability plastic or ceramic packages.

Did you find this article useful? Share it!

Join the circuit, keeping you connected to OnlineComponents.com and beyond!